Tool/software:
Hello TI,
I designed the sound card with PCM2903CDB (bought from mouser).
I noticed at first turn ON and testing that PCM2903C successfully connect to laptop (USB AUDIO CODEC), picture below. Then I test HID control and this also worked. I saw in windows notification that volume changed or muted.

After interface tests I found big problem that when I pressed play some music on laptop, the analog output not working. There is constant 3.3V level and nothing change. Measured on the IC side, on pins 16 and 15.After capacitor there was "zero".

Also, I measured it with AC setting in scope. In the picture below, is the measured waveform, but it will be only "noise".

Digital out (S/PDIF) seemed to work. I am not able to test with some audio device. I only measured the waveform with scope. Check picture below...
Only connected device (turned on), the music is not played.

Second scope screen, when music played. I know this is maybe hard to confirm that is working but you can see that waveform is different / denser.

Have you encountered anything similar? The IC is soldered properly without short or cold junction (picture below). Xtal is clocking correctly.
It is such a simple connection that there is no reason why it should not work. I'm quite disappointed with that. Is it possible that Mouser sold me a faulty/damaged PCM2903CDB?

PCM2903CDB schematic circuit below. Power port 3V3_VDD is from LDO and USB_C_VBUS is 5V from USB port. I did the tests without connected additional circuits to confirm that the problem is only in the PCM2903CDB.

Thank you for support.
Best regards,
Martin