Part Number: OPA1652
Other Parts Discussed in Thread: OPA1688, OPA1656, INA849, JFE150
Tool/software:
I'm designing the input stage for a guitar input and have identified the OPA1652 as a good candidate, but I have a question.
The Vcm in the datasheet is (V–) + 0.5 (V+) – 2. I will likely power this from a 9V supply split to ±4.5V, Sure, a typical guitar output should not go near the rails, however a humbucker pickup with heavy gauge strings might, or powered by a 9V battery that is 30% depleted you might get near, and its always good to have some leeway.
So my question is, if the input does run into the top 2V, will this clip harshly, or will it simply impede the datasheet quoted performance? Might seem like a silly question, but the OPA1688 datasheet has the sentence, "Note that this device can operate with full rail-to-rail input 100 mV beyond the top rail, but with reduced performance within 2 V of the top rail."
That info is very useful information for a designer, and maybe I'll select the OPA1688 for this application: I could design for 95% of the guitars in the world, knowing that if I get a really hot signal, my device will still work as planned (and if the signal is that hot, I doubt many people will notice the slight drop in THD). Initially, I favoured a FET-input op-amp for this application, but I note that the OPA1688 has a very high input impedance; since it's CMOS architecture I guess it's MOSFET rather than FET or JFET input; so it could work really well. It seems like an underrated device!
I'm aware that I could add a discrete FET source follower stage and then use a more general rail-to-rail op-amp after that, and I may end up doing that, but since I need an op-amp stage in this circuit anyway I might as well explore the possibility of using that for input.
Cheers.