Tool/software:
Hi team,
The datasheet mentions AEC-Q100 Qualified for automotive applications– Temperature grade 1: –40°C to 125°C, TA --- This refers to the ambient temperature of the working environment, right?
We would like to know, when the ambient temperature is 125 degrees Celsius, what is the Junction temperature of the AMP chip under full power working state?
The Junction temperature is 155~170 degrees Celsius --- This means that the chip will shut down for self-protection after the Junction temperature reaches 155. What is the limit temperature of full performance? --- We understand that the chip should have performance regression after reaching a certain high temperature, and then shut down after the Junction temperature reaches 155. We would like to know at what temperature the chip will no longer run at full performance?