Tool/software:
Hi Sir,
We encountered an issue with the Tas5825M when running an input sample rate of 96kHz. No audio output was heard from the chip. However, when we reduced the input to 48kHz, the audio output was restored. We would like to know if there are any specific settings required for the Tas5825M when operating with a 96kHz input
Thanks
Welson