Hi,
I would like to ask a question on TLV320AIC23B, document SLWS106H.
I see for both input and output pins there are two modes: (1)Line (2) Mic (headphone). For output, the nominal output level for both modes are 1.0 VRMS, however:
1. For line out, it is just plain 1.0 VRMS.
2. For Mic(headphone), it is marked as 0-dB output level, and there are gain between -73dB to 6dB for adjustment
Mic output seems to have the added capability of output level adjustment. Is this the only difference? Why for line output there is no such adjustment? Is it because:
I am not quite sure on it. Could anyone explain on the differences?
Zheng