Tool/software:
I am trying to test the TLV320DAC3100EVM-U kit with IMX93QS93 Linux board. I am able to detect it know as you can see here:
root@qs93-5210:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: tlv320aic31xxco [tlv320aic31xx-codec], device 0: 443b0000.sai-tlv320dac31xx-hifi tlv320dac31xx-hifi-0 [443b0000.sai-tlv320dac31xx-hifi tlv320dac31xx-hifi-0] Subdevices: 1/1 Subdevice #0: subdevice #0
and,
root@qs93-5210:~# aplay -L null Discard all samples (playback) or generate zero samples (capture) sysdefault:CARD=tlv320aic31xxco tlv320aic31xx-codec, 443b0000.sai-tlv320dac31xx-hifi tlv320dac31xx-hifi-0 Default Audio Device
- But when I tried to aplay sine wave I got the following errors:
root@qs93-5210:~# speaker-test -D plughw:0,0 -c 2 -r 48000 -F S16_LE -t sine -f 500 speaker-test 1.2.8 Playback device is plughw:0,0 Stream parameters are 48000[ 247.600154] tlv320aic31xx-codec 1-0018: aic31xx_setup_pll: Sample rate (48000) and format not supported Hz, S16_LE, 2 ch[ 247.610738] tlv320aic31xx-codec 1-0018: ASoC: error at snd_soc_dai_hw_params on tlv320dac31xx-hifi: -22 annels Sine wave[ 247.621511] 443b0000.sai-tlv320dac31xx-hifi: ASoC: error at __soc_pcm_hw_params on 443b0000.sai-tlv320dac31xx-hifi: -22 rate is 500.0000Hz Rate set to 48000Hz (requested 48000Hz) Buffer size range from 32 to 131072 Period size range from 16 to 8184 Using max buffer size 131072 Periods = 4 Unable to set hw params for playback: Invalid argument Setting of hwparams failed: Invalid argument
- I've seen this related kernel messages as well:
alsa-lib /usr/src/debug/alsa-lib/1.2.8-r0/src/ucm/main.c:1541:(snd_use_case_mgr_open) error: failed to import hw:0 use case configuration -2 No state is present for card tlv320aic31xxco alsa-lib /usr/src/debug/alsa-lib/1.2.8-r0/src/ucm/main.c:1541:(snd_use_case_mgr_open) error: failed to import hw:0 use case configuration -2 Found hardware: "simple-card" "" "" "" "" Hardware is initialized using a generic method
- Here it is my device tree :
audio_clk: audio-clk { compatible = "fixed-clock"; #clock-cells = <0>; clock-frequency = <12288000>; }; codec_audio: sound { compatible = "simple-audio-card"; simple-audio-card,name = "tlv320aic31xx-codec"; simple-audio-card,format = "i2s"; simple-audio-card,bitclock-master = <&codec_dai>; simple-audio-card,frame-master = <&codec_dai>; simple-audio-card,widgets = "Microphone", "Mic Jack", "Line", "Line In", "Line", "Line Out", "Headphone", "Headphone Jack", "Speaker", "Speaker Out"; simple-audio-card,routing = "Line In", "AIN1", // Line input route "Line Out", "HPL", // Line out to left headphone "Line Out", "HPR", // Line out to right headphone "Headphone Jack", "HPL", "Headphone Jack", "HPR"; status = "okay"; cpu_dai: simple-audio-card,cpu { sound-dai = <&sai1>; }; codec_dai: simple-audio-card,codec { sound-dai = <&audio_codec>; clocks = <&audio_clk>; }; }; }; &sai1 { #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_sai1>; status = "okay"; assigned-clocks = <&clk IMX93_CLK_SAI1>; assigned-clock-parents = <&clk IMX93_CLK_AUDIO_PLL>; assigned-clock-rates = <12288000>; clocks = <&clk IMX93_CLK_SAI1_IPG>, <&clk IMX93_CLK_AUDIO_PLL>, <&clk IMX93_CLK_DUMMY>, <&clk IMX93_CLK_DUMMY>, <&clk IMX93_CLK_AUDIO_PLL>; clock-names = "bus", "mclk1", "mclk2", "mclk3", "pll"; }; &lpi2c2 { clock-frequency = <400000>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_lpi2c2>; status = "okay"; // Add TLV320AIC3100 audio codec node audio_codec: codec@18 { compatible = "ti,tlv320dac3100"; pinctrl-names = "default"; reg = <0x18>; #sound-dai-cells = <0>; reset-gpio = <&gpio4 9 GPIO_ACTIVE_LOW>; HPVDD-supply = <®_vdd_3v3>; AVDD-supply = <®_vdd_3v3>; DVDD-supply = <®_vref_1v8>; IOVDD-supply = <®_vdd_3v3>; SPRVDD-supply = <®_vdd_3v3>; SPLVDD-supply = <®_vdd_3v3>; status = "okay"; }; };
I am struggling to make this work, could anyone help me out with this?