Tool/software:
Hello there,
We are using the TLV320ADC6140 to collect 1 analog mic input and 4 PDM microphone streams and output over TDM. We would like to add PCM audio from another device as I2S input/output to the TDM bus using the the free GPI/GPO pins in daisy-chain mode. Is this doable?
In the PPC3 app for the eval board it looks like I can set GPI to "ASI Input for Daisy Chain - SDIN" and GPO1 to "Secondary ASI Output (SDOUT2)". Is this correct?
Essentially, my PCM audio device supports I2S but not TDM, so I would like to bring the data lines into the ADC and add it to the TDM bus. Then I would assume that I would simply share the TDM frame clock and bit clock to that PCM audio device directly set to slave mode. Is this how the daisy chain function works?
Thanks so much!
Peter Grinalds