Other Parts Discussed in Thread: TLV320ADC5120, TAA5212
Tool/software:
Hi expert,
We would like to set the PCM4202 to PCM slave Mode, Quad Rate and operate the Sampling Rates at 210.9kHz.
In this case, tLRCKP=4.748us(=1/210.9kHz) tBCKP=74.19ns(=tLRCKP/64). Are there any violations ?
Refer to the Datasheet
P14(,etc...) states that the maximum Sampling Rate is 216kHz, so We think 210.9kHz is within the range.
On the one hand, figure 6 states that tLRCKP=MIN 5us (tBCKP= MIN 78ns),
We are confused because the maximum Sampling Rates can be read as 200kHz(=1/5us).