Part Number: OPA1612
Tool/software:
We have an OPA1612AIDRGR Op-Amp that has failed in a circuit, drawing too much current.
I tried to remove another IC from a working circuit using hot air ~400°C to replace the failed one.
Both are drawing around 40mA (12V supply) with nothing connected to the other pins.
Looking at the datasheet, the maximum quiescent current should be no more than 10mA.
I assume the high heat has likely caused damage and resulted in the high current consumption on the part removed to replace the faulty one?
I am yet unsure what caused damage to the original faulty part in-circuit?