This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1622: EN (Shutdown not working)

Part Number: OPA1622
Other Parts Discussed in Thread: OPA1632

Tool/software:

Hello,

I am using the OPA1622 in a design as unity gain buffer, as shown below.

The Enable pin is normally pulled up to 34V1 (34V) using a 22k resistor. Then I have an external switch that connects the EN pin to GND. When the switch is engaged the votlage on the enable pin is 0.077V (77mV).

The amplifier does go into a low power state however any input signal is also showing up on the output but with very high distortion.

So to me, it seems like the amplifier is not being fully turned off there is some bleed though. Is this normal behavior?

To me, it seems like the amplifier should be completely shut down and nothing should pass through it from input to output.