This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5441-Q1: schematic review

Part Number: TAS5441-Q1


Tool/software:

Hi Team,

Please review Samsung schematic and feedback as below quesitons.

TAS5441_SS_Oct_10.pdf

Need to guide for shunt cap bsed on VIN

    - considering to use 5W (4ohm) Speaker and 9.5V VIN based on Line impedance, Inductor DCR, Cable.

RL

RS

Vp (=PVDD)

Pout (W at 10% THD)

Ivrms

4.00

0.20

5.38

2.99

0.86

4.00

0.20

9.50

9.32

1.53

4.00

0.20

14.40

21.42

2.31

In case of 9.5V VIN, please guide Min shunt cap & series inductor (330uF and 10uH size are is too much for layout) 

Best regards

Joey Kim

  • Hi Joey,

    The schematic is good, with one observation:  If the audio source is a differential output, you do not need the 49.9kOhm resistors to ground.  (R1282 and R1285)

    The 330uF can be as low as 100uF, but you will see more ripple on your power supply.  The 10uH inductor can be changed to meet your EMC requirements.

    Regards,
    Gregg Scott