This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424L-Q1: TDM Clock Error

Part Number: TAS6424L-Q1


Tool/software:

Hi There,

I intend to use the TAS6424L-Q1 with a TDM signal from a MCHstreamer (MiniDSP). TDM 8 @96 kHz on 24 bits.

DI Timing and values requirement seem 100% compatible.

As soon as activated (mute or play mode) the clock error occurs and no signal is sent to the speaker.

Using either MCLK or SCLK (as suggested in the documentation)  for both MCLK and SCLK doesn't change anything.

TAS6424L-Q1 was tested using the USB audio input as well the Optical input with the MCHstreamer. Both work fine.

Thanks for your help

Laurent