Tool/software:
Hello E2E Experts,
Good day.
I recently was approved to get the PurePath Console 3 software in order to interface with my PCM6360Q1EVM-PDK and AC-MB boards; however, it says I have no available apps to install. I'm not sure how else to interact with the boards if I can't install the necessary application software.
I did see the FAQ earlier;
[FAQ] PUREPATHCONSOLE: How to Install PurePath︎ Console 3 Device Apps Manually
However, I can't see a tar.gz file for the version 3.2.0 download which is the one I installed. There is one for v3.0.8.alpha.2, but I'm unsure if these would be compatible.There also seems to be 2 tar.gz files under the 3.0.8.alpha.2 download. One is ppc3.tar.gz, and the other is ppc3_darwin.tar.gz.
Is this the correct file to use, or is there another one I'm not seeing?
Regards,
TI-CSC