This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805M: What's the min height value of TAS5805M

Part Number: TAS5805M
Other Parts Discussed in Thread: TAS5805

Tool/software:

Hi, Team

Customer is checking with us about the min_height value of the TAS5805.As you can see from the datasheet as below, TAS5805M didn’t have such value. TAS5805M only have max_height which is 1.2mm.

But from our another device TAS5828, the min_height value is 1.00.

Could u help to check the min_height value of the TAS5805M?

Thanks.

G.W

  • hi, G.W

    usually, you can consider 10% variance.

    if you worry about the heatsink dimension, we recommend set that between 1-1.2 will be better.

    this can make the heatsink contact with chip much better.

    tks

    jesse