Tool/software:
I can't see this on the data sheet - what are the current source/sink specs. for the 4 digital output pins? I need to drive an opto relay that
needs about 15mA.
TIA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I can't see this on the data sheet - what are the current source/sink specs. for the 4 digital output pins? I need to drive an opto relay that
needs about 15mA.
TIA
Hi Ian,
The GPO digital output current drive capability of the PGA2500 is limited. The typical digital high-level output drive current capability at (VA+) - 1.0V is Io = 200μA, and the the typical digital low-level output sink current capability at 0.4V is Io = -3.2mA. Please see typical spec under Digital Characteristics, on the VOH/VOL spec test conditions on page 3:

Therefore, unfortunately, the PGA2500 will not be able to drive/control directly the opto relay that consumes about 15mA, you will need to use a digital buffer with the current drive capability.
Thank you and Kind Regards,
Luis