Tool/software:
1. Is it sufficient to use a 10uF capacitor to ground when the actual power consumption of the speaker is 10W on one side at PVDD=20V for the TAS5825M chip?
2. Is there any hidden danger in using 10uH + 0.68uF LC filter combination for the speaker?