Tool/software:
In the process of using the TPA3111D1, there is a problem: during the operation of the device, there is suddenly no sound.
The schematic diagram is as follows, loaded with a 4Ω speaker:

Here are a few questions I would like to confirm
- Is there a relationship curve between temperature and output efficiency? The fault is prone to low temperatures of -20°C.
- Is PLIMIT a power limiting function, is it the average power or instantaneous power that is restricted?
- How does the chip determine the SC failure? Is it to detect the voltage and current at the output? What is the threshold for SC failures?
- TThe typical output power is 10W, regardless of signal quality, is there a maximum and minimum index?