Part Number: TAS5805M
Tool/software:
Hi,
In our project, we're using the TAS5805M in BTL mode with a maximum output of 1W per channel.
However, when PVDD is set to 24V, the temperature rises above 150°C until the amp triggers thermal protection.
We’ve confirmed that the software initialization sequence is correct,
So we’re a bit confused about to why the temperature is so high, even with such a low output.
Could you provide any suggestions? What options are available to reduce the temperature? For example, parameter settings, etc.
Thank you!