Tool/software:
Hi TI team,
Following up on this Class H issue in the TAS6584- here is the issue I posted about previously:
A proper Class H tracking supply (or a Class H control signal like that created in the TAS6584) should be subject to the output signal of the datapath (sent to the audio amplifier) rather than the input signal. It seems that the TAS6584 does not behave in this manner. I am unsure whether it is a bug or it if we are not properly configuring the TAS6584.
Here is the test that we performed that showed this errant behavior:
- We set the lower and upper boundary of power supply range to 5VDC and 14VDC, respectively, in the PPC3 GUI.
- Holding the volume control of the TAS6584 to 0dB, we varied the amplitude of the input signal from -10dB to +10dB, and monitored the tracking signal.
- The Class H control signal changed with the input signal
- Once the range of the tracking signal was established- we left the input level fixed and used the TAS6584 volume control to attenuate the output of the TAS6584 device.
- The Class H control signal did not change.
This behavior renders the volume control of the TAS6584 unusable if the product is to reap the benefits of Class H operation. With that said, if the volume control at the output of the digital audio is not used, the dynamic range of the complete audio data path is compromised because the audio processing in the TAS6584 is executed on an attenuated signal.
I am attaching a PPT file to this thread for your review and a screenshot of the summary is shown below:
Can you please confirm that this is the expected behavior of the TAS6584? If not, what I2C control registers can be used to correct the behavior of the TAS6584?
Looking forward to your response.