This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3140:Resolution Jump and Output Nonlinearity in ADC with Differential Sine Wave Input

Part Number: TLV320ADC3140


Tool/software:

ADC に正弦波を入力すると、期待どおりの解像度が得られないという問題が発生しています。これについてアドバイスをお願いします。

私の ADC 設計には大きな問題があります。非線形性チェック0b0000: 出力に大きなジャンプがあり、特に MSB 4 ビットがまたはのみを表示する問題があります0b1111。アドバイスをお願いします。

  • 動作モード: スレーブモード

  • 電源電圧: 3.3V

  • 入力タイプ:差動入力フルスケールAC信号電圧

  • 出力長: 24ビット

  • データ形式: 左揃え (LJ)

  • 極性: 単極性

  • 基準電圧(Vref):2.75V

# Differential 1-channel : INP1/INM1 - Ch1 # FSYNC = 96 kHz (Output Data Sample Rate), BCLK = 6 MHz (BCLK/FSYNC = 64) ################################################################ # # # Power up IOVDD and AVDD power supplies keeping SHDNZ pin voltage LOW # Wait for IOVDD and AVDD power supplies to settle to steady state operating voltage range. # Release SHDNZ to HIGH. # Wait for 1ms. # # Wake-up device by I2C write into P0_R2 using internal AREG w 98 02 81 # # set LJ-Mode, 24 bits word length w 98 07 A0 # # Enable Line input, Typical 10-kΩ input impedance w 98 3C 84 # # Enable Input Ch-1 I2C write into P0_R115 w 98 73 80 # # Enable ASI Output Ch-1 to Ch-4 slots by I2C write into P0_R116 w 98 74 80 # # Power-up ADC and PLL by I2C write into P0_R117 w 98 75 60 # # Apply FSYNC = 96 kHz kHz and BCLK = 6 MHz MHz and # Start recording data by host on ASI bus with LJ protocol 24-bits channel wordlength