This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Now I do not have TAS5805MEVB in hand, how can I adjust the sound effect through PPC3, can I output the bin file through other methods?
Can I adjust the sound through PPC3 output bin file without TAS5805MEVM?
我是否可以通过PPC3输出bin文件来调整音效,在没有TAS5805MEVM的条件下?
hi
we cannot realize that by bin file.
current tas5805 can only export .h file which can be used for tuning.
tks
jesse
Hello,
The .h file has a list of the registers and values that need to be written and some example code in the top of the file. The registers when written will configure the device according to how it was set up in PPC3.
Regards,
Ramsey