Tool/software:
Dear Ti experts,
I am currently converting the PWM signal from a Class-D headphone amplifier into an analog signal through an LPF and then input it to the TPA6132.
According to the TPA6132 datasheet, the input signal needs to meet the requirement of Vpkpk being less than 2.2V, which I can achieve by adjusting the volume. However, I would like to know if there are any other requirements for the input signal, such as frequency, etc.?