Tool/software:
Hello, I have a question about the LM4871MMX/NOPB circuit.
The circuit is configured as shown in the attached image.
The problem is that Pop Up noise occurs when power is supplied.
In order to solve the Pop Up Noise, I lowered the audio amp input capacitor value from 390 -> 10nF and conducted a test.
The Pop Up Noise sound was confirmed to be reduced, but the overall volume of the amp also decreased.
I designed it based on the reference circuit in the datasheet, but it was not resolved.
The speaker uses CDS-4410-54SP of cui device, and the main specifications are as follows.
1. Impedance: 4 ohm
2. Max power: 6W
I would like to ask which part should be modified, so please reply.