TPA3139D2EVM: How to solve speaker not playing music?

Part Number: TPA3139D2EVM
Other Parts Discussed in Thread: TLV320AIC3254, TPA2012D2EVM

Tool/software:

Hi, 

I am an intern from a sports-related company, and I have been given a task to use TPA3139D2EVM and connect to a speaker to play sound from a computer.

Previously I had use TLV320AIC3254 which connects to TPA2012D2EVM which connects to the speaker and had successfully play music from my computer. However, the music was quite soft, so I was told to swap TPA2012D2EVM with TPA3139D2EVM hopefully to have a louder sound output from the speaker. The speaker specs are 1.5W, 8ohms. 

I am not using the RCA jack and had soldered the input signal cable directly on C24 and C25 capacitors.

The issue is there is incoming signal to TPA3139D2EVM, but the speaker is not outputting any sound. I am supplying 5V, 7ampere to the board and not using plimit. Is there any way to solve this issue?

Thank you.

Best Regards,

Samuel