Other Parts Discussed in Thread: TAS6424
Tool/software:
Hi TI,
We want to verify if the tas6424 to speaker pathway is function well. Can you provide the configuration of registers related to generating sine waves. tks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi TI,
We want to verify if the tas6424 to speaker pathway is function well. Can you provide the configuration of registers related to generating sine waves. tks.
Hi Jin
Write 0x80 to register 0x1D, clear fault.
Write 0x2A to register 0x28, as datasheet requested.
Write 0x00 to register 0x04, to set PLAY.
If all of the working condition is meet, the device should start working.
Suggest you to use PPC3 software for the initialization design, especially helpful when you meet problem and want to debug.
Hi Robert
Please follow both below link, to request the PPC3 software, and TAS6424 APP.
Hi Shadow,
We measured the TDM signal through an oscilloscope. May I ask if the register configuration is correct.
0x0 0x0
0x1 0x32
0x2 0x62
0x3 0x4
0x4 0x0
0x5 0xff
0x6 0xff
0x7 0xff
0x8 0xff
0x9 0x0
0xa 0x11
0xb 0x11
0xc 0x0
0xd 0x0
0xe 0x0
0xf 0x55
0x10 0x0
0x11 0x0
0x12 0x0
0x13 0x20
0x14 0xff
0x15 0x0
0x16 0x0
0x17 0x0
0x18 0x0
0x19 0x0
0x1a 0x0
0x1b 0x0
0x1c 0x0
0x1d 0x0
0x1e 0x0
0x1f 0x0
0x20 0x0
0x21 0x0
0x22 0x1
0x23 0x14
0x24 0x0
0x25 0x0
0x26 0x40
0x27 0x26
0x28 0xa
0x77 0x0
0x78 0x3f
0x79 0x0


Hi Robert
The SCLK frequency shows you are using TDM8, and FSYNC only has 1bit clock. What is the MCLK frequency you are using? If it is the same with SCLK, you may need to take care of below requirement in the datasheet:

About the register, 0x28 register is the one you should take care, datasheet says must set to 0x2A. Others just function related, set them as you needed.