Other Parts Discussed in Thread: TPA2005D1
Tool/software:
Hello, I'm a beginner on audio projects and I have many doubts:
I want to amplify 3 outputs of the PCM4104 (working at 24bit and 192kHz) because the sound isn't that loud.
PCM4104 is driving 3 mono channels: 2 of them connected to headphones and the other one to a bone transducer. The three of them have 10Ohm of impedance and I want to be able to deliver 1W maximum.
The schematic is basically a copy:
of the one recommended on PCM4104's datasheet: Figure 21. Single-Ended Output Filter Circuit:
The only differences are the Opamp IC and the rail voltages.
Would the TPA2005D1 amplifier be enough for this purpose (one amplifier for channel)?
also, I don't understand how to correctly connect:
the output of the PCM4104 to the input of the TPA2005D1
the output of TPA2005D1 and the input of the jack
Thanks for your support!