Other Parts Discussed in Thread: OPA134
Tool/software:
HI, staff
In Rev.C, the Trim terminal has been removed and changed to an NC terminal,
so I would like to check the terminal processing method.
OPA132 データシート(SBOS0504C)
The Pin Configuration and Functions describes how to connect NC-pins, but I have an additional question.
1-pin : Do not connect these pin.
(1) Existing layouts for the OPA132 before revision C of this data sheet do not need to be redesigned.
Q1→ A Trim resistor is connected in the user's existing circuit.
Is it necessary to delete the circuit?
Is it okay to connect it without deleting the existing circuit?
8-pin : No internal connection. Float this pin.
Q2→ A Trim resistor is connected in the user's existing circuit.
Do I need to delete the circuit?
Is it okay to connect it without deleting the existing circuit?
regards
cafain