Hi,
I'm trying to program mini DSP in ADC3101 because I need click remove function adding on PRB2.


So, I nned to change to use miniDSP instead of PRB2.
Now, I'm trying to just implement PRB2 by using Purepath.
1. Choose Framework ADC3x01App4x_1
2. Choose MonoDec4xIn_1 with AGC enable
3. cascade 5 biquad
4 connect to MonoI2S_out.
However, it seems to works as different as PRB2.
Here is the question,
1.While choosing MonoDec4xIn_1, does it means that I'm choosing "Decimation Filter A" and I don't have to add any component on Purepath GDE?
2. Does the AGC setting in MonoDec4xIn_1 is in the end of the 5 biquad Filtesr? Just like PRB2 or it is in from]nt of all?
Thanks for your help first.