This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC1110: About output signals

Part Number: TLV320AIC1110


Tool/software:

Hi team,

I would like to route the output of EAR2 to MIC1P,N and output on PCMOUT.
However, due to the rule of input full scale voltage, I cannot use the output of EAR2 as it is, so I will input the output of EAR2 with -20dB externally.
After that, it is assumed that 29.5dB amplification is performed in the TLV320AIC1110 and PCMOUT is output.
In this case, does this mean that the audio output is 8.95dB higher than the original data?

Best Regards,
Ryu.