Tool/software:
Amplifier channels are not going to plya state after channels fault removed at runtime
1.Amplifier put in play state
Channel State Control Register (address = 0x04) configured with 0x00 value in all the channels in play state. It worked as expected.
2.Auto diagnostic enabled for channel fault monitoring run time(Cyclic)
DC Load Diagnostic Control 1 Register (address = 0x09) configured bit0 to 0(Auto diag enable) value.
3.Create the fault any one channel and fault(Short to bat or Short to GND) reported correctly.
DC Load Diagnostic Report 1 Register (address = 0x0C)
4. But after remove the channel fault, Channel should be go to play state but here channel is not going to play state and its in DC load diagnostic.
Channel State Reporting Register (address = 0x0F)