Part Number: PCM1690
Tool/software:
Hi,
The customer needs to use 16 channels. Can we cascade 2pcs to achieve this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM1690
Tool/software:
Hi,
The customer needs to use 16 channels. Can we cascade 2pcs to achieve this?
Hello,
The BCK limit per datasheet is BCK(max)=1/40n==> 25MHz . To use 16 channel of data ( and assuming 48KHs sampling rate and 24bit data) your BCK has to run as
16x24x48K=18.432MHz which is within the spec. So from outside of the device, if you can manage to feed the data accordingly to 2 PCM1690 that are in parallel , then you can get the 2 groups of 8 channels( or simply 16channels) of data.
Regards,
Arash