Other Parts Discussed in Thread: DRV601, TLV320DAC3100, TAD5242, PCM5102
Tool/software:

Hi,
I have this requirement where I need to store .WAV file in our system and my system shall be capable to play the stored .wav file using a headphone which has an impedance of 600Ω. Need help in selecting a suitable Audio DAC and Amplifier. Detailed explanation is as below.
We have a small duration .wav file, we are planning to use a SPI Flash to store this .wav file. But .wav file may need to be converted into a format such as PCM? To store it in external Flash, can this be done?.
If we are able store the audio .wav file in required format in SPI flash, my FPGA shall be will read and route it to Audio DAC using I2S protocol, DAC will decode the digital format of the audio data to a analog signal.
Since we need to drive the headphone with an impedance of 600Ω,we may need amplifier to achieve this? Hence would Line driver DRV601 be a good suite for this kind of application?
Thanks in advance.