Part Number: TAS5825M
Other Parts Discussed in Thread: TAS5828M
Tool/software:
I would like to use the TAS5825M or TAS5828M without purchasing the EVM for PurePath (PPC3). I am aware that I cannot use certain features like the SmartAmp since they need to characterise the speaker with the EVM but i am willing to not use those features. Therefore I have two questions:
- Is it possible to use these devices on a custom PCB without using PPC3 at all, therefore completely without all DSP features of the device?
- Is it possible to use PPC3 for certain specific features, such as EQs, and creating a config file that I can upload to the device via I2C without purchasing an EVM?
Thank you already in advance.