Tool/software:
I am having difficulty using the TAC5212EVM-K configured for mono output
I am configuring it via PPC, and set it to use the OUT1M using the USB audio interface to let me do some basic stability testing with Windows.
I generated a 32-bit 48000Hz sample rate 75Hz sine wave audio file being played back. The signal is not distorted in the software (Audacity) and it is properly configured for 32-bit 48000Hz playback. The TI driver on the lower right icons is there, and was also set to 32-bit output.
When I configure the output to have a gain of -8dB (dropdown, not slider) I see a bad signal that certainly looks like half of a differential output (below).
With lower output gain selected (dropdown not slider), it instead produces a higher amplitude fully clipped square wave. Yes, when I *decrease* the output amplitude in the program, it *increases* the output amplitude and causes it to turn into a square wave (below).
I see it constantly rail the output regardless of the volume control setting in Audacity, Windows, the TI icon on the tray, or the PPC software.
I can only guess that some jumper must be wrong, but the eval board documentation doesn't show the full audio path and is transparently wrong -- at a bare minimum J59 and J60 are not even four pin header. We don't know how to tell what's incorrect, but it all seems fine when we slowly read the datasheet. I attached photos showing the configuration of the output for reference.
Please let us know if you have any hints, thanks. I'd love to be able to consider using this part but this is rough for a basic performance check. All I was looking to do was measure the AC voltage stability... which at present is not even measurable.