Part Number: TAD5242
Other Parts Discussed in Thread: TAC5242, , TAD5212, TAC5212
Tool/software:
I'm looking to use the TAC5242 in a new design connected to a Raspberry Pi over I2S. In my design I need both unbalanced and balanced outputs concurrently, I don't want the user to have to choose (with jumpers), but have both active at the same time. Preference would be to have standard 1Vrms lineout on the unbalanced output, and professional level +4 dBu on the balanced output, two channels (stereo). Sound quality is more important than cost at this point, however PCB real estate is limited, so using an active opamp for the output may be the best option (dual channel if available). Also I only have 3.3V power supply available.
Thanks,
/Hakan