Part Number: TAC5112
Other Parts Discussed in Thread: TAC5242, , TAS2505, TLV320AIC3100, TLV320AIC3120, TAC5142
Tool/software:
Our customer is considering use of TAC5112 or possible TAC5242 and has a few questions:
- Are there any suggestions, best practices, or app notes when using the on-board headphone amplifier to drive headphones directly?
- How can I use several of these parts on the same TDM audio bus? Is there a limit to how many I can use? I need at least 4. Maybe 5. Each will individual audio channels. The datasheet alluded to this being possible, but it isn’t super clear to me how this is done.
- Lastly, we need to drive a speaker as well… Legacy could drive 2W into a 4ohm speaker. What is the right way to do that? Should I use the TAC5xxx + a dedicated analog speaker amp? Or do you have a DAC with a small speaker amp built in? the curveball to that route is it needs to live on the same TDM audio bus, so multi-channel compatibility is necessary.
Thank you!