Part Number: TLV320AIC3253
Other Parts Discussed in Thread: TAS2552, LM48310
Tool/software:
TLV320AIC3253 When in MAST mode, is the MCU host available without MCLK? How to design it if it is paired with LM48310 or TAS2552?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
To design with LM48310 or TAS2552 (or any analog input amplifier) couple the Line Outputs from the codec to the analog inputs of the amp with a 1st order low pass filter fc = 20kHz.
In Master Mode the source clock must be present for the codec to operate correctly. BCLK can be a substitute if MCLK is not available.

Best regards,
Jeff McPherson
Hi,
AIC3253 can act as Master to output BCLK but it requires a source clock (like MCLK). See this app note for recommended configurations when dealing with master/slave modes: https://www.ti.com/lit/an/slaa469a/slaa469a.pdf?ts=1735919390258&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTLV320AIC3253
Best regards,
Jeff McPherson