Part Number: PCM1754
Other Parts Discussed in Thread: PCM1794
Tool/software:
Dears,
SCH

Configure as FMT=0


Customer's processor is ADSP-21565, with a main clock frequency of 12.288MHz (connected to the main clock input of PCM1794), and is also connected to ADSP-21565,21565 to generate I2S bit clock (1.024MHz) and synchronous clock (16kHz) through frequency division, as shown in the following figure

The data output of I2S remains at a low level, as shown in the following figure

There is a problem where the I2S data output is low and there is a large amount of noise in the simulated output (as shown in the figure below). Could you please help me figure out what is going on? Thank you