Tool/software:
Dear TI experts,
My customer wants to use chip inductor instead of power inductor on the output.
Could you conform that it is okay?
- AUDIO SPEC - 14.4±0.5V, 20±15˚C, 4ohm ,1W , 1KHz
|
1. FREQUENCY RESPONSE(EQ Flat) |
1kHz |
Ref. |
|
127Hz |
0±3 dB |
|
|
10007Hz |
0±3 dB |
|
|
2. SN RATIO |
1kHz |
≥ 60dB |
|
3. THD |
1KHz |
≤ 0.5% |
|
4. CH SEPARATION |
1kHz |
≥ 50dB |
|
10kHz |
≥ 50dB |
|
|
5. MAX Power |
10% T.H.D |
≥ 20W |

They want to change L4012 and L4014 to chip inductor.
They saw the document SLOA242, there are some results using chip inductor.

Please check this issue. Thanks.
Best regards,
Chase