Tool/software:
Hello!
We are planning to use the TLV320AIC3101 as audio ADC in one of our projects.
Therefore we've got the TLV320AIC3101EVM-K evaluation board which includes the USB-MODEVM motherboard.
To test the settings of the CODEC we use the USB Interface to record audio on the computer.
Unfortunatly we get quite high noise of around -50dbFS as soon as we enable the PGA.
We've already enabled the high-pass filter which improved the noise but no matter which setting we tested we couldn't get to noise below -50dbFS.
Since the datasheet says that the SNR of the ADC is around 92dB, we wonder how or if you can achive that with the evaluation board.
Thanks,
Philipp