This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3100: MIC0RP ADC to I2S_DOUT

Part Number: TLV320AIC3100


Tool/software:

I connected a microphone to MIC0RP. I want to transmit this microphone via bluetooth with i2s by passing it through the ADC. I made the necessary register settings in the block diagram. I wrote 01 to the d7-d6 bits in the P1/49 register, meaning "CM is selected for the MIC PGA with feed-forward resistance RIN = 10 kΩ."
I wrote 01 to the d5-d4 bits in the P1/48 register, meaning "MIC1RP is selected for the MIC PGA with feed-forward resistance RIN = 10 kΩ"
My mic gain in the P1/47 register is 14.5 dB.
After these settings, don't I need to read the data coming from the microphone when I read with an oscilloscope on the dout pin of the codec? I tried and verified that the microphone works with the analog bypass. I have now turned off the analog bypass. When I read from Dout with an oscilloscope, there is a continuous data but it does not change according to the movement in the microphone. Do I have a mistake on the I2S side (frequency, sample rate settings) or am I missing a setting that I should have set beforehand?


blue signal is TLV320AIC3100 dout pin
purple signal is din pin, din pin is working properly. When i send music or voice signal, purple signal changes. Now i send no signal so it's normal.

  • Hi Hamza,

    Mic signals are quite soft, and so it will be hard to monitor the I2S signal on a scope for meaningful changes. We recommend using an I2S analyzer to plot the data as it will give more meaningful results.

    Another option is to use a function generator in place of the mic so that you have a larger signal that will create more variations in the I2S data.

    Best regards,
    Jeff McPherson