Tool/software:
Hi TI experts,
I'm currently developing board using TPA3116 chip in PBTL mode. I would like to know how to implement the bootstrap snubbers on this configuration. On the EVM schematic I saw that in PBTL mode the output P & N are tied together, so can I use just 1 snubber on each channel (one for OUT+ and one for OUT-). If this is possible, then what's the recommended value? Should I keep 330pF & 10R, or should I use the parallel value from both bootstrap snubbers? 680pF & 5R1 perhaps?
Regards,
Salwa