Tool/software:
I am trying to configure the TLV320ADC6140 as a master, outputting FCLK @ 48KHz and BCLK @ 3.072MHz (x64) on an I2S output.
1 - I looked in the datasheet and did not see that I had to use an MCLK input, but I am guessing I do in master mode. Can someone confirm this?
2 - If I use the TI eval PCB and SW for this device and wire the I2C to configure my device, I see FCLK = 46.2KHz and the PLL config shows it should be 96KHz (photo below). I am not sure what to do at this point. Any suggestions or questions that might help understand this and help me get the 48KHz FCLK I desire. As noted in the photo, my MCLK is external at 12MHz.