This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6584-Q1: output amplitude with PCM2706

Part Number: TAS6584-Q1
Other Parts Discussed in Thread: PCM2706,

Tool/software:

I'm using a PCM2706 to generate the I2S input for TAS6584-Q1 and created the initial register configuration with PPC3 with the following settings:

  • I2S, 4CH BTL 48KHz 16bit 64Fs
  • PWM 384KHz, BD modulation, 
  • SDOUT disabled
  • Class H OFF.
  • Thermal foldback OFF.
  • Clip detect OFF.
  • Gain compensation OFF.
  • PVDD foldback OFF.

Power is 12V.

When I send a 100% amplitude sinewave to the PCM2706 I see it severely clipped at the outputs.

I need to set the digital volume (registers 0x40-0x43) to approximately 0x48 (=-12dB gain) in order for the sinewave to use most 0-12V output range without being clipped.

I do not understand why 0dB gain results in a clipped sinewave. I thought 0dB meant that the full range of 16 bit sample values would cover the full PVDD output range (with some distortion and clipping due do 100% duty cycle not being possible).

Any help understanding why I need to set -12dB just to not get my waveform clipped would be much appreciated.

Thanks.

  • Ignacio,

    The analog gain is set to you can adjust the gain of the power amplifier section of the device.  We allow for the audio to clip so we can have 10% THD.  You can adjust the volume or the analog gain to meet your needs.

    Regards,
    Gregg Scott