If we use cc8520 in host controlled master mode, what is the default volume setting?
Vlad
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If we use cc8520 in host controlled master mode, what is the default volume setting?
Vlad
Hi Vlad,
The default / start-up is mute.
This is the sequence you need to run:
NWM_ACH_SET_USAGE(0x00,0x01,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff,0xff)
VC_SET_VOLUME(0,0,1,0,1,0,0xFFF0)
First one will map logic audio channel to local audio interface channels. Second will unmute and set volume.
Hope this helps.
Kjetil