This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5822M: TAS5822M tuning tool, the position of the EQ can affect the output noise.

Part Number: TAS5822M

Tool/software:

Dear expert:

Could you help on below technical issue?   

Test conditions: PVDD = 24V, speaker load: 4Ω@PBTL mode  

The following two PPC3 files have the same parameter configurations except for the positions of the EQs. The observed phenomena are as follows:

- **Noise OK file**: EQ4 and EQ9 are turned off, while EQ12 and EQ13 are used. The output noise is 0.4mV (A-wt).
- **Noise NG file**: EQ4 and EQ9 are used, while EQ12 and EQ13 are turned off. The output noise is 0.7mV (A-wt).

Questions to be addressed:
1. Why does the position of the EQ affect the output noise?
2. Are there any guideline documents for EQ tuning?

Nosie NG.ppc3

Nosie OK.ppc3