Part Number: PCM1840EVM
Tool/software:
We have a customer who is requesting the following regarding part number: PCM1840EVM.
"I am interested in part number: PCM1840EVM
A few questions:
0. Does the board do 4 ch at 192kHz sample rate for each channel?
0.5 The microphone inputs look like 'balanced' inputs - the differential
amplifier is on-board the EVM kit?
0.6 If so, is the diff amp circuit usable/licenseable IP?
1. Is it possible to 'clock synch' two or more of these boards?
1.5 How are they physically connected to do that?
2. Is there a software spec/example on how to get the digital audio
samples off the board?
3. Is there a path to production from the TI EVM kit? As in, how crazy is
it to go to fab on our own PCB boards, taking this kit as a reference?
4. What other licensing has to be taken into account in order to go from
this board to custom production?
Thanks much! I hope my question numbering scheme was taken at least as an
attempt at levity ..."