This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5805M: Register check

Part Number: TAS5805M
Other Parts Discussed in Thread: TAS5805

Tool/software:

Hi Ti team,

During the debugging of the TAS5805M device, we found that it could operate normally when the PVDD supply voltage was 12V; however, when the PVDD supply voltage was raised to 24V, the power amplifier would trigger a protection mechanism. After adjusting the relevant register parameters, the device could resume normal operation under a 24V supply condition. Now, we would like to ask for your assistance in reviewing whether the following register configuration is reasonable to ensure the stability and reliability of the system. Thank you for your support!

/*
 * Copyright (c) Huawei Technologies Co., Ltd. 2020-2020. All rights reserved.
 * description: function define
 * author: audio
 * create: 2020-10-29
 */

/******************************* include files *******************************/
/* unf headers */
#include "hi_log.h"
#include "hi_common.h"
#include "hi_drv_sys.h"

/* drv headers */
#include "hi_type.h"
#include "drv_amp_private.h"
#include "drv_amp_ioctl.h"
#include "hi_drv_amp.h"
#include "drv_amp_ext.h"
#include "amp_i2s.h"

#ifdef __cplusplus
#if __cplusplus
extern "C" {
#endif
#endif /* __cplusplus */

#define ENDTBL_FLAG           0xff
#define AMP_DEBUG             0
#define MAX_AMP_REG_LEN       20
#define TAS5805_DRC_VAL_LEN   4
#define TAS5805_PEQ_VAL_LEN   4
#define TAS5805_INIT_INTERVAL 65   /* delay 65ms */
#define INVALID_GPIONUM       0xff
#define INIT_DELAY 5

#define TAS5805M_REG_00 0x00
#define TAS5805M_REG_03 0x03
#define TAS5805M_REG_35 0x35
#define TAS5805M_REG_7F 0x7f

#define TAS5805M_PAGE_00 0x00
#define TAS5805M_BOOK_00 0x00

static amp_global_param *g_tas5805_drv = HI_NULL;

typedef struct {
    hi_u8 addr;
    hi_u8 value;
} tas5805_regmap;

static tas5805_regmap g_tas5805_init_sequence[] = {
    { 0x00,        0x00 },
    { 0x7f,        0x00 },
    { 0x03,        0x03 },
    { 0x78,        0x80 },
    { ENDTBL_FLAG, 0x00 },
};

static hi_s32 amp_tas5805_set_mute(hi_bool mute);

static hi_s32 amp_write_reg(hi_u8 u1_addr, hi_u8 *u1_buf, hi_u16 u2_byte_cnt)
{
    hi_s32 ret;

    check_amp_func_init(g_tas5805_drv);
    check_amp_func_init(g_tas5805_drv->p_i2c_func);
    check_amp_func_init(g_tas5805_drv->p_i2c_func->pfn_i2c_write);

    ret = g_tas5805_drv->p_i2c_func->pfn_i2c_write(g_tas5805_drv->i2c_num,
        g_tas5805_drv->device_addr,
        u1_addr, 1, u1_buf, u2_byte_cnt);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 i2c write error\n");
        hi_err_print_h32(g_tas5805_drv->i2c_num);
        hi_err_print_h32(g_tas5805_drv->device_addr);
        hi_err_print_h32(u1_addr);
        hi_err_print_h32(u1_buf[0]);
        hi_err_print_h32(u2_byte_cnt);
    }

    return ret;
}

static hi_s32 amp_read_reg(hi_u8 u1_addr, hi_u8 *u1_buf, hi_u8 max_len, hi_u16 u2_byte_cnt)
{
    hi_s32 ret;

    check_amp_func_init(g_tas5805_drv);
    check_amp_func_init(g_tas5805_drv->p_i2c_func);
    check_amp_func_init(g_tas5805_drv->p_i2c_func->pfn_i2c_read);

    ret = g_tas5805_drv->p_i2c_func->pfn_i2c_read(g_tas5805_drv->i2c_num,
        g_tas5805_drv->device_addr,
        u1_addr, 1, u1_buf, u2_byte_cnt);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 read fail!\n");
        hi_err_print_err_code(ret);
    }

    return ret;
}

static hi_void amp_power_up(hi_bool power)
{
    hi_s32 ret = HI_SUCCESS;

    if (g_tas5805_drv == HI_NULL) {
        HI_LOG_ERR("TAS5805 no init! \n");
        return;
    }

    if (g_tas5805_drv->p_gpio_func == HI_NULL) {
        HI_LOG_ERR("GPIO function null \n");
        return;
    }

    if (g_tas5805_drv->reset_gpio_num == INVALID_GPIONUM) {
        HI_LOG_WARN("the amp TAS5805 unsupported reset!\n");
        return;
    }

    if (g_tas5805_drv->p_gpio_func->pfn_gpio_dir_set_bit != HI_NULL) {
        ret = g_tas5805_drv->p_gpio_func->pfn_gpio_dir_set_bit(g_tas5805_drv->reset_gpio_num,
            g_tas5805_drv->gpio_output_polarity);
        if (ret != HI_SUCCESS) {
            HI_LOG_ERR("call pfn_gpio_dir_set_bit fail!\n");
            hi_err_print_err_code(ret);
            return;
        }

        msleep(1);
    }

    if (g_tas5805_drv->p_gpio_func->pfn_gpio_write_bit != HI_NULL) {
        if (power) {
            ret = g_tas5805_drv->p_gpio_func->pfn_gpio_write_bit(g_tas5805_drv->reset_gpio_num,
                g_tas5805_drv->reset_polarity);
        } else {
            ret = g_tas5805_drv->p_gpio_func->pfn_gpio_write_bit(g_tas5805_drv->reset_gpio_num,
                !(g_tas5805_drv->reset_polarity));
        }

        if (ret != HI_SUCCESS) {
            HI_LOG_ERR("call pfn_gpio_write_bit fail!\n");
            hi_err_print_err_code(ret);
            return;
        }

        msleep(TAS5805_INIT_INTERVAL);
    }

    return;
}

static hi_void amp_tas5805_hw_mute(hi_bool mute)
{
    hi_s32 ret;

    ret = amp_tas5805_set_mute(mute);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("set_mute failed!\n");
    }
}

static hi_s32 amp_tas5805_init(amp_global_param *amp_drv)
{
    hi_s32 ret;
    hi_u8 index = 0;
    hi_u8 addr = 0;
    hi_u8 value = 0;
    tas5805_regmap *tas5805_init_sequence = g_tas5805_init_sequence;

    check_amp_null_ptr(amp_drv);

    g_tas5805_drv = amp_drv;

    msleep(INIT_DELAY);
    amp_power_up(HI_TRUE);
    msleep(INIT_DELAY);

    for (index = 0;; index++) {
        addr = tas5805_init_sequence[index].addr;
        if (addr == ENDTBL_FLAG) {
            break;
        }

        value = tas5805_init_sequence[index].value;

        ret = amp_write_reg(addr, &value, 1);
        if (ret != HI_SUCCESS) {
            HI_LOG_ERR("TAS5805 init fail \n");
        }

#if AMP_DEBUG
        hi_u8 read_array[MAX_AMP_REG_LEN] = { 0 };
        ret = amp_read_reg(addr, read_array, MAX_AMP_REG_LEN, 1);
        hi_dbg_print_h32(addr);
        hi_dbg_print_h32(read_array[0]);
        HI_LOG_DBG("\n");
#endif
    }

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_resume(amp_global_param *amp_drv)
{
    return amp_tas5805_init(amp_drv);
}

static hi_void amp_tas5805_de_init(hi_void)
{
    if (g_tas5805_drv == HI_NULL) {
        /* delete print to a hi_void rmmod error print while tas5805 is not initialized. */
        return;
    }

    /* power down AMP */
    amp_power_up(HI_FALSE);

    g_tas5805_drv = HI_NULL;
}

static hi_s32 amp_tas5805_set_mute(hi_bool mute)
{
    hi_s32 ret;
    hi_u8 i;
    hi_u8 addr = 0;
    hi_u8 value = 0;
    hi_u8 reg03_value = 0;
    hi_u8 reg35_value = 0;

    /* sequence need to write 5 registers */
    tas5805_regmap mute_sequence[5] = {
        { TAS5805M_REG_00, TAS5805M_PAGE_00 },
        { TAS5805M_REG_7F, TAS5805M_BOOK_00 },
        { TAS5805M_REG_00, TAS5805M_PAGE_00 },
        { TAS5805M_REG_03, 0x03 },
        { TAS5805M_REG_35, 0x11 },
    };

    check_amp_func_init(g_tas5805_drv);

    if (mute) {
        /* mute both left & right channels */
        reg03_value = 0x0b;
        reg35_value = 0x00;
    } else {
        /* unmute */
        reg03_value = 0x03;
        reg35_value = 0x11;
    }

    mute_sequence[3].value = reg03_value; /* the 3th value write to reg TAS5805M_REG_03 */
    mute_sequence[4].value = reg35_value; /* the 4th value write to reg TAS5805M_REG_35 */

    /* sequence need to write 5 registers */
    for (i = 0; i < 5; i++) {
        addr = mute_sequence[i].addr;
        value = mute_sequence[i].value;

        ret = amp_write_reg(addr, &value, 1);
        if (ret != HI_SUCCESS) {
            HI_LOG_ERR("TAS5805 write mute reg fail!\n");
            return ret;
        }
    }

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_get_mute(hi_bool *mute)
{
    hi_s32 ret;
    hi_u8 gain = 0;

    check_amp_func_init(g_tas5805_drv);

    ret = amp_read_reg(TAS5805M_REG_35, &gain, 1, 1);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 read mute reg fail!\n");
        return ret;
    }

    if (gain == 0x00) {
        *mute = HI_TRUE;
    } else {
        *mute = HI_FALSE;
    }

    return HI_SUCCESS;
}

static hi_s32 amp_set_drc_en(hi_bool en)
{
    hi_s32 ret;
    hi_u8 i;
    hi_u8 addr = 0;
    hi_u8 value = 0;
    hi_u8 drc_val[TAS5805_DRC_VAL_LEN] = { 0 };

    /* sequence need to write 4 registers */
    tas5805_regmap sequence[4] = {
        { TAS5805M_REG_00, TAS5805M_PAGE_00 },
        { TAS5805M_REG_7F, TAS5805M_BOOK_00 },
        { TAS5805M_REG_00, TAS5805M_PAGE_00 },
        { 0x66, 0x00 },
    };

    check_amp_func_init(g_tas5805_drv);

    ret = amp_read_reg(0x66, drc_val, TAS5805_DRC_VAL_LEN, 1);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 read drc reg fail!\n");
        return HI_FAILURE;
    }

    if (en == HI_TRUE) {
        drc_val[0] &= ~0x02; /* BIT1 = 0 NOT bypass DRC */
    } else {
        drc_val[0] |= 0x02; /* BIT1 = 1 bypass DRC */
    }

    sequence[3].value = drc_val[0]; /* the 3th value write to reg 0x66 */

    /* sequence need to write 4 registers */
    for (i = 0; i < 4; i++) {
        addr = sequence[i].addr;
        value = sequence[i].value;

        ret = amp_write_reg(addr, &value, 1);
        if (ret != HI_SUCCESS) {
            HI_LOG_ERR("TAS5805 write drc reg fail!\n");
            return ret;
        }
    }

    return HI_SUCCESS;
}

static hi_s32 amp_get_drc_en(hi_bool *en)
{
    hi_s32 ret;
    hi_u8 drc_val[TAS5805_DRC_VAL_LEN] = { 0 };

    check_amp_func_init(g_tas5805_drv);

    ret = amp_read_reg(0x66, drc_val, TAS5805_DRC_VAL_LEN, 1);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 read drc reg fail!\n");
        return ret;
    }

    if ((drc_val[0] & 0x02) == 0x02) { /* BIT1 = 1 bypass DRC */
        *en = HI_FALSE;
    } else {
        *en = HI_TRUE;
    }

    return HI_SUCCESS;
}

static hi_s32 amp_set_peq_en(hi_bool en)
{
    hi_s32 ret;
    hi_u8 i;
    hi_u8 addr = 0;
    hi_u8 value = 0;
    hi_u8 peq_val[TAS5805_PEQ_VAL_LEN] = { 0 };

    /* sequence need to write 4 registers */
    tas5805_regmap sequence[4] = {
        { TAS5805M_REG_00, TAS5805M_PAGE_00 },
        { TAS5805M_REG_7F, TAS5805M_BOOK_00 },
        { TAS5805M_REG_00, TAS5805M_PAGE_00 },
        { 0x66, 0x00 },
    };

    check_amp_func_init(g_tas5805_drv);

    ret = amp_read_reg(0x66, peq_val, TAS5805_PEQ_VAL_LEN, 1);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 read peq reg fail!\n");
        return ret;
    }

    if (en == HI_TRUE) {
        peq_val[0] &= ~0x01; /* BIT0 = 0 not bypass EQ */
    } else {
        peq_val[0] |= 0x01; /* BIT0 = 1 bypass EQ */
    }

    sequence[3].value = peq_val[0]; /* the 3th value write to reg 0x66 */

    /* sequence need to write 4 registers */
    for (i = 0; i < 4; i++) {
        addr = sequence[i].addr;
        value = sequence[i].value;

        ret = amp_write_reg(addr, &value, 1);
        if (ret != HI_SUCCESS) {
            HI_LOG_ERR("TAS5805 write peq reg fail!\n");
            return ret;
        }
    }

    return HI_SUCCESS;
}

static hi_s32 amp_get_peq_en(hi_bool *en)
{
    hi_s32 ret;
    hi_u8 peq_val[TAS5805_PEQ_VAL_LEN] = { 0 };

    check_amp_func_init(g_tas5805_drv);

    ret = amp_read_reg(0x66, peq_val, TAS5805_PEQ_VAL_LEN, 1);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5707 read peq reg fail!\n");
        return ret;
    }

    if ((peq_val[0] & 0x01) == 0x01) { /* BIT0 = 1 bypass EQ */
        *en = HI_FALSE;
    } else {
        *en = HI_TRUE;
    }

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_set_sub_woofer_vol(hi_u32 volume)
{
    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_get_sub_woofer_vol(hi_u32 *volume)
{
    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_check_reg_addr(hi_u32 reg_addr)
{
    if (reg_addr > ENDTBL_FLAG) {
        HI_LOG_ERR("invalid reg addr\n");
        hi_err_print_h32(reg_addr);
        return HI_FAILURE;
    }
    return HI_SUCCESS;
}

static hi_void amp_tas5805_check_byte_size(hi_u32 *byte_size)
{
    if (*byte_size > MAX_AMP_REG_LEN) {
        HI_LOG_ERR("TAS5805 reg length MAX is 20\n");
        *byte_size = MAX_AMP_REG_LEN;
    }
}

static hi_s32 amp_tas5805_write_reg(hi_u32 reg_addr, hi_u32 byte_size, HI_VIRT_ADDR_T value_vir_addr)
{
    hi_s32 ret;
    hi_u8 reg_array[MAX_AMP_REG_LEN] = { 0 };

    check_amp_func_init(g_tas5805_drv);

    ret = amp_tas5805_check_reg_addr(reg_addr);
    if (ret != HI_SUCCESS) {
        return ret;
    }
    amp_tas5805_check_byte_size(&byte_size);

    ret = copy_from_user(reg_array, (hi_u8 *)(uintptr_t)value_vir_addr, byte_size);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 copy_from_user fail \n");
        return ret;
    }

    ret = amp_write_reg(reg_addr, (hi_u8 *)reg_array, byte_size);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 write I2C fail \n");
        return ret;
    }

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_read_reg(hi_u32 reg_addr, hi_u32 byte_size, HI_VIRT_ADDR_T value_vir_addr)
{
    hi_s32 ret;
    hi_u8 reg_array[MAX_AMP_REG_LEN] = { 0 };

    check_amp_func_init(g_tas5805_drv);

    ret = amp_tas5805_check_reg_addr(reg_addr);
    if (ret != HI_SUCCESS) {
        return ret;
    }
    amp_tas5805_check_byte_size(&byte_size);

    ret = amp_read_reg(reg_addr, reg_array, MAX_AMP_REG_LEN, byte_size);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 read I2C fail \n");
        return ret;
    }

    ret = copy_to_user((hi_u8 *)(uintptr_t)value_vir_addr, reg_array, byte_size);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("TAS5805 copy_to_user fail \n");
        return ret;
    }

    return HI_SUCCESS;
}

static hi_void amp_tas5805_read_proc_base(hi_void *p)
{
    HI_CHIP_VERSION_E chip_version = HI_CHIP_VERSION_BUTT;
    HI_CHIP_TYPE_E chip_type = HI_CHIP_TYPE_BUTT;

    hi_drv_sys_get_chip_version(&chip_type, &chip_version);

    osal_proc_print(p,
        "\n==============================================hi3751v%x AMP PROC===="
        "==========================================\n",
        (hi_u32)chip_version);
    osal_proc_print(p, "AMP modul:        TI TAS5805\n");
    osal_proc_print(p, "I2C num:          %d\n", g_tas5805_drv->i2c_num);
    osal_proc_print(p, "I2C addr:         0x%x\n", g_tas5805_drv->device_addr);
    osal_proc_print(p, "mute  GPIO group: %d\n", g_tas5805_drv->hw_mute_gpio_num / AMP_GPIO_BITS_PER_GROUP);
    osal_proc_print(p, "mute  GPIO bit:   %d\n", g_tas5805_drv->hw_mute_gpio_num % AMP_GPIO_BITS_PER_GROUP);
    osal_proc_print(p, "mute  polarity:   %d\n", g_tas5805_drv->hw_mute_polarity);
    osal_proc_print(p, "reset GPIO group: %d\n", g_tas5805_drv->reset_gpio_num / AMP_GPIO_BITS_PER_GROUP);
    osal_proc_print(p, "reset GPIO bit:   %d\n", g_tas5805_drv->reset_gpio_num % AMP_GPIO_BITS_PER_GROUP);
    osal_proc_print(p, "reset polarity:   %d\n", g_tas5805_drv->reset_polarity);
}

static hi_s32 amp_tas5805_read_proc(hi_void *p, hi_void *data)
{
    hi_s32 ret;
    hi_bool mute_en = HI_FALSE;
    hi_bool drc_en = HI_FALSE;
    hi_bool peq_en = HI_FALSE;

    check_amp_func_init(g_tas5805_drv);
    amp_tas5805_read_proc_base(p);

    osal_proc_print(p,
        "\n-------------------------------------------------TAS5805 STATUS-------"
        "------------------------------------------\n");

    ret = amp_tas5805_get_mute(&mute_en);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("AMP get_mute failed!\n");
    }

    osal_proc_print(p, "MUTE: %s\n", mute_en ? "ON" : "OFF");

    ret = amp_get_drc_en(&drc_en);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("AMP get_drc_en failed!\n");
    }

    osal_proc_print(p, "DRC: %s\n", (drc_en) ? "ON" : "OFF");

    ret = amp_get_peq_en(&peq_en);
    if (ret != HI_SUCCESS) {
        HI_LOG_ERR("AMP get_peq_en failed!\n");
    }

    osal_proc_print(p, "PEQ: %s\n", (peq_en) ? "ON" : "OFF");

    osal_proc_print(p,
        "============================================================"
        "====================================================\n");

    osal_proc_print(p, "get setting command:   echo help > /proc/msp/amp\n");

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_get_enanle(hi_bool *set_en, char *cmd)
{
    if (strstr(cmd, "1")) {
        *set_en = HI_TRUE;
    } else if (strstr(cmd, "0")) {
        *set_en = HI_FALSE;
    } else {
        return HI_FAILURE;
    }
    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_proc_set_mute(unsigned int argc, char (*argv)[PROC_CMD_SINGEL_LENGTH_MAX])
{
    hi_s32 ret;
    hi_bool get_en = HI_FALSE;
    hi_bool set_en = HI_FALSE;

    if (argc != 2) {    /* 2 is argc num. */
        return HI_FAILURE;
    }

    ret = amp_tas5805_get_mute(&get_en);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    ret = amp_tas5805_get_enanle(&set_en, argv[1]);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    ret = amp_tas5805_set_mute(set_en);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    osal_printk("set amp mute %s success:%d(%s) -> %d(%s)\n",
        (set_en ? "ON" : "OFF"), (hi_u32)get_en,
        (get_en ? "ON" : "OFF"), (hi_u32)set_en, (set_en ? "ON" : "OFF"));

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_proc_set_drc(unsigned int argc, char (*argv)[PROC_CMD_SINGEL_LENGTH_MAX])
{
    hi_s32 ret;
    hi_bool get_en = HI_FALSE;
    hi_bool set_en = HI_FALSE;

    if (argc != 2) {    /* 2 is argc num. */
        return HI_FAILURE;
    }

    ret = amp_get_drc_en(&get_en);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    ret = amp_tas5805_get_enanle(&set_en, argv[1]);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    ret = amp_set_drc_en(set_en);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    osal_printk("set amp drc %s success:%d(%s) -> %d(%s)\n",
        (set_en ? "ON" : "OFF"), (hi_u32)get_en,
        (get_en ? "ON" : "OFF"), (hi_u32)set_en, (set_en ? "ON" : "OFF"));

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_proc_set_peq(unsigned int argc, char (*argv)[PROC_CMD_SINGEL_LENGTH_MAX])
{
    hi_s32 ret;
    hi_bool get_en = HI_FALSE;
    hi_bool set_en = HI_FALSE;

    if (argc != 2) { /* 2 is argc num. */
        return HI_FAILURE;
    }

    ret = amp_get_peq_en(&get_en);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    ret = amp_tas5805_get_enanle(&set_en, argv[1]);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    ret = amp_set_peq_en(set_en);
    if (ret != HI_SUCCESS) {
        return HI_FAILURE;
    }

    osal_printk("set amp peq %s success:%d(%s) -> %d(%s)\n", (set_en ? "ON" : "OFF"),
        (hi_u32)get_en,
        (get_en ? "ON" : "OFF"), (hi_u32)set_en, (set_en ? "ON" : "OFF"));

    return HI_SUCCESS;
}

static hi_s32 amp_tas5805_write_proc(amp_cmd_proc cmd, unsigned int argc,
    char (*argv)[PROC_CMD_SINGEL_LENGTH_MAX], hi_void *private)
{
    check_amp_func_init(g_tas5805_drv);

    if (cmd == AMP_CMD_PROC_SET_MUTE) {
        if (amp_tas5805_proc_set_mute(argc, argv) != HI_SUCCESS) {
            goto CMD_FAULT;
        }
    }

    if (cmd == AMP_CMD_PROC_SET_DRC) {
        if (amp_tas5805_proc_set_drc(argc, argv) != HI_SUCCESS) {
            goto CMD_FAULT;
        }
    }

    if (cmd == AMP_CMD_PROC_SET_PEQ) {
        if (amp_tas5805_proc_set_peq(argc, argv) != HI_SUCCESS) {
            goto CMD_FAULT;
        }
    }

    if (cmd == AMP_CMD_PROC_SET_HELP) {
        amp_proc_show_help();
    }

    return HI_SUCCESS;

CMD_FAULT:
    HI_LOG_ERR("proc cmd is fault\n");
    amp_proc_show_help();

    return HI_FAILURE;
}

amp_drv_func g_tas5805_func = {
    .b_ext_m_clk_flag = HI_FALSE,
    .amp_read_proc = amp_tas5805_read_proc,
    .amp_write_proc = amp_tas5805_write_proc,
    .amp_read_reg = amp_tas5805_read_reg,
    .amp_write_reg = amp_tas5805_write_reg,
    .amp_get_sub_woofer_vol = amp_tas5805_get_sub_woofer_vol,
    .amp_set_sub_woofer_vol = amp_tas5805_set_sub_woofer_vol,
    .amp_get_mute = amp_tas5805_get_mute,
    .amp_set_mute = amp_tas5805_set_mute,
    .amp_deinit = amp_tas5805_de_init,
    .amp_init = amp_tas5805_init,
    .amp_resume = amp_tas5805_resume,
    .amp_hw_mute = amp_tas5805_hw_mute,
    .amp_soft_reset = HI_NULL,
};

amp_drv_func *amp_get_tas5805_func_handle(hi_void)
{
    return &g_tas5805_func;
}

#ifdef __cplusplus
#if __cplusplus
}
#endif
#endif /* end of #ifdef __cplusplus */