Other Parts Discussed in Thread: TLV320ADC3140
Tool/software:
Hello,
We have verified SNR on TAA3020EVM.
Here is the result.
Differential input: 106dB with 0dB gain, 98dB with +20dB gain, it is 8dB degradation
SE AC input: 99dB with 0dB gain, 81dB with +20dB gain, it is 18dB degradation
What is reason SE mode create 10dB more degradation?
It seems that is not caused by front end amp NF performance.
Regards,
Mochizuki