Part Number: TLV320AIC34
Tool/software:
Hello Abigail Leonardi .
I am seeing an issue with the setup of the codec in which registers 79, 86 and 93 are reading "Not all programmed gain have been applied" (D1 bit is set) when I attempt to set the Output level control to 0dB, unmute, and power on the respective lines.
I can't seem to determine why I am seeing this. I have also ensured in our setup that ADC flags, DAC status and power status are ok
| Register # | ADDR_A | ADDR_B |
| 79 | 0x00 | 0x0B |
| 86 | 0x0B | 0x00 |
| 93 | 0x0B | 0x00 |